Redesigned Mobile App for Emerson’s SCADA in the Cloud Drives More Efficient, Optimized Operations

DeltaV™ SaaS SCADA Mobile App

Emerson's new DeltaV™ SaaS SCADA Mobile empowers operators and technicians to do more in the field from their mobile devices. High Resolution Image

DeltaV SaaS SCADA mobile app updated to empower operators and technicians with more visibility, awareness and customization options regardless of location

AUSTIN, Texas (July 14, 2025) – Emerson, an industrial technology leader delivering advanced automation solutions, has redesigned the mobile app for its DeltaV™ SaaS supervisory control and data acquisition (SCADA) software. The new app will empower operators and technicians to do more in the field from their mobile devices, helping teams in critical industries like oil and gas, specialty chemical and others achieve more efficient, optimized operations.

Operators and field technicians increasingly rely on mobile applications for SCADA solutions to help them monitor and manage production on the go, manually input data, change settings and issue commands and simplify the work of recording chart estimates from anywhere across a plant or facility. However, today’s most efficient and effective teams need more robust mobile applications and a user-friendly interface to allow them to do more from anywhere. The redesigned mobile app for DeltaV SaaS SCADA is designed to give operators and technicians the control and clarity they need to be effective in the field, without the need to drag a laptop along with them.

The rebuilt DeltaV SaaS SCADA mobile app provides an entirely redesigned user interface (UI) for more intuitive viewing of critical operations information. Via the new UI, users can create and customize their own reports, allowing them to compare multiple sensors and locations to have better visibility into how operations are working in the field. The new UI also delivers alarms via push notifications, helping ensure operators and technicians are made aware of problems as quickly as possible.

Users also gain access to new route planning features. They can create and manage routes/runs on the fly directly from the mobile app, making it easier to customize runs to their specific schedules and daily plans. An operator or technician can view the stops on the route at any time to quickly see which are in alarm and can seamlessly pass location information directly to the mobile device’s mapping app to be guided to locations.

“Today, many operators and technicians are using mobile devices as their primary interface to their SCADA systems,” said Nina Golder, vice president of Emerson’s Guardian software and solutions business. “We’ve redesigned the DeltaV SaaS SCADA mobile app from the ground up to provide that mobility—delivering a more seamless, intuitive way for users to access all the key information they need, in the format they desire, from anywhere across their plant, facility, or enterprise.”

DeltaV SaaS SCADA’s mobile app also features new widgets to simplify operation, making it easy for users to quickly see total alarms for selected locations and comparison of volumes produced.


Media:
• Contacts: Emerson Global Media Contacts

Additional resources:
• Join the Emerson Exchange 365 Community
• Connect with Emerson via X Facebook LinkedIn YouTube
• Visit Emerson’s Industrial Software Page on LinkedIn
• Visit Emerson’s DeltaV Automation Platform Page on LinkedIn

About Emerson
Emerson (NYSE: EMR) is a global industrial technology leader that provides advanced automation. With an unmatched portfolio of intelligent devices, control systems and industrial software, Emerson delivers solutions that automate and optimize business performance. Headquartered in St. Louis, Missouri, Emerson combines innovative technology with proven operational excellence to power the future of automation. For more information, visit Emerson.com.

Włącz skrypt JavaScript aby skorzystać z tej strony internetowej.