Emerson’s New Edge Device Simplifies SCADA Architecture

DeltaV SaaS SCADA with Edge Connect

The DeltaV™ SaaS SCADA with Edge Connect unlocks secure communication to all field devices using their native protocols. High Resolution Image

The DeltaV SaaS SCADA with Edge Connect edge solution combines the power of edge computing with the flexibility of a cloud platform
 

AUSTIN, Texas (April 29, 2025) – Emerson, an industrial technology leader delivering advanced automation solutions, has released DeltaV™ SaaS SCADA with Edge Connect, a flexible, preconfigured edge solution engineered to deliver more seamless operational technology (OT) data mobility out of the box. Designed to connect existing field devices to the cloud-hosted DeltaV SaaS Supervisory Control and Data Acquisition (SCADA) system in minutes, the DeltaV SaaS SCADA with Edge Connect edge solution eliminates much of the traditional engineering work necessary to bring critical operational data into the control system for better visibility and safer, more flexible and reliable control.  

“DeltaV SaaS SCADA with Edge Connect advances Emerson’s Boundless Automation vision of seamless data mobility from the intelligent field, through the edge, and into the cloud,” said Nina Golder, vice president of Emerson’s Guardian software and solutions business. “Designed with open protocols and preconfigured with the most advanced edge technology stack available, the DeltaV SaaS SCADA with Edge Connect edge solution empowers users to remotely monitor and configure their field assets, bringing visibility and operations online in minutes while still providing powerful capabilities to customize their experience.”

Built on Emerson’s PACEdge™ software for edge computing, the DeltaV SaaS SCADA with Edge Connect edge solution can communicate with all field devices—remote terminal units, flow computers, valves, sensors and more—in their native protocols using an Emerson-tested third-party polling engine that eliminates the need for additional conversion or adapters. PACEdge provides an IIoT application enablement platform designed to integrate information technology and OT domains without disrupting OT assets, architectures or systems.

All software necessary to connect and run the edge solution is preinstalled on the device, and additional applications can be added via a built-in marketplace. In addition, users can also build and add their own custom containerized applications with built-in Node-RED, a low-code programming platform for event-driven applications. 

Built in alignment with International Society of Automation 62443 standards and the European Union’s Cyber Resilience Act, the DeltaV SaaS SCADA with Edge Connect edge solution provides a secure platform for industrial operations. It also provides report by exception capabilities, allowing the device to automatically switch polling frequencies for increased communication when a new value is registered from a device in the field, helping teams maintain critical visibility without increasing bandwidth and communication costs. Data buffering features allow the DeltaV SaaS SCADA with Edge Connect edge solution to store data during communication outages and send them when communication is restored so no data is lost. Dynamic polling resolution automatically changes polling rates when events occur, helping ensure all critical data is delivered promptly.

The DeltaV SaaS SCADA with Edge Connect edge solution will be on display at Emerson Exchange 2025, being held May 19-22 in San Antonio, Texas.

Media:
• Contacts: Emerson Global Media Contacts

Additional resources:
• Join the Emerson Exchange 365 Community
• Visit Emerson’s Industrial Software Page on LinkedIn
• Visit Emerson’s DeltaV Automation Platform Page on LinkedIn
• Connect with Emerson via X Facebook LinkedIn YouTube

About Emerson
Emerson (NYSE: EMR) is a global industrial technology leader that provides advanced automation. With an unmatched portfolio of intelligent devices, control systems and industrial software, Emerson delivers solutions that automate and optimize business performance. Headquartered in St. Louis, Missouri, Emerson combines innovative technology with proven operational excellence to power the future of automation. For more information, visit Emerson.com.

Włącz skrypt JavaScript aby skorzystać z tej strony internetowej.