Flow measurement of natural gas

Measurement of the standard volume flow (with DGM functionality) of natural gas on a compressor station
Flow measurement of natural gas

Measuring and calculation of gas standard volume flow at compressor station

Gas transport means transmission from the production sites to the consumption area to feed gas into the distribution networks there. The gas transport network can be compared to a motorway as it is made up of large axes, while the distribution networks are made up of shorter axes that route the gas directly to the consumer. At a national level, long-distance pipelines of the gas transport network efficiently connect the storage caverns or aquifers with the distribution networks. A key requirement for the smooth functioning of the infrastructure is information about the gas volumes that flow from one region to another or from one company to another. 

The non-intrusive ultrasonic measuring system measures accurately standard volume flow incorporating Dynamic Gas Meter (DGM) functionality for direct compressibility factor, density and molar weight calculation, bypassing the need for extensive additional instrumentation.

Read More...
Click to continue reading Measuring and calculation of gas standard volume flow at compressor station
Please enable JavaScript to use this website.