AMS 2140 Machinery Health Analyzer Compatibility
AMS 2140 adjoins other AMS condition monitoring hardware like AMS Wireless Vibration Monitor, AMS Asset Monitor, AMS 6500 ATG, and AMS 9420 Wireless Vibration Transmitter, under one, consolidated software system.
Previously, the AMS 2140 required the use of AMS Machinery Manager, the legacy predecessor to the more advanced AMS Machine Works platform. This setup often involved switching between software systems, managing more licenses, and other extra tasks.
Portable Device Agent
AMS Machine Works v1.8 includes a new Portable Device Agent, a lightweight service that enables your laptop to sense when your AMS 2140 connects to the USB port. Once the device is sensed and discovered by your laptop, AMS 2140 communication is then routed to the AMS Machine Works server. Now, you’ll be ready to transfer routes and condition monitoring data from your AMS 2140 to the AMS Machine Works database. Additionally, the service will also support Wi-Fi and Ethernet communication.
Routes
Traditional route-based condition monitoring is a proactive approach to asset management where maintenance technicians or engineers use portable diagnostic tools to regularly collect data from rotating machinery (like pumps, motors, gearboxes, and others), following a predefined, pre-loaded route of equipment to be monitored around a facility or process unit – a method that has been used for decades. The primary goal is to detect early signs of equipment failure and avoid unexpected breakdowns by analyzing vibration, temperature, and other operational parameters. Just as they have done for years in AMS Machinery Manager, AMS 2140 users will now be able to configure and modify routes in AMS Machine Works v1.8, as well as setting analysis parameters and alarms.
Design Studio
Version 1.8 incorporates a more user-friendly design, while also offering users of previous iterations of AMS Machine Works (and AMS Machinery Manager) reasonable levels of familiarity they can build on as they unlock value with the many new features and benefits. Conversely, brand new users of the software will find version 1.8 an advantageous starting point due the highly intuitive, user-assisting nature of the software. This improvement reflects Emerson’s commitment to a human-centered design approach.
This becomes especially clear when configuring your machines in the Machine Train Builder module. Here, you’ll find an intuitive drag-and-drop diagramming tool, a more streamlined design workflow, redesigned menus, and an extensive library of specialized asset types—with domain expertise embedded into the fabric of the software.
Machine building and configuration will greatly increase capacity to support many more assets within one machine train. Version 1.8 will add custom fault frequencies, the ability to set more alarms per measurement point, short and transient waveform collection for AMS 6500 ATG, and more customization for analysis parameters.
New Dashboards and Analysis Interfaces
A Landing Page Built for Efficiency
AMS Machine Works’ new dashboard offers a powerful combination of data accessibility, intuitive navigation, and advanced analysis tools, user-friendly design, advanced prioritization capabilities, and a more seamless workflow, enabling maintenance teams to work smarter, not harder. The new landing page in AMS Machine Works functions as a centralized hub, giving users an at-a-glance view of essential KPIs and tools that are frequently accessed. The design reflects modern code and user-focused approach, organizing information into intuitive panels that highlight top priorities right from the start. This design ensures that, from the moment you log in, you’re presented with the data that matters most.
Prioritizing Assets by Criticality and Alarms
One of the standout features of this dashboard is its dynamic prioritization system. If the user has provided an asset criticality ranking, the software can detect alarms in real time, multiply the asset criticality score by the alarm criticality, and generate a list of equipment ranked by urgency. This functionality makes it simple to identify which machine trains or pieces of equipment need immediate attention—ensuring that the most critical issues are at the top of your to-do list. This prioritization tool helps maintenance teams focus their efforts where it matters most, potentially preventing costly breakdowns or extended downtime.
Effortless Workflow from Landing Page to Detailed Dashboards
AMS Machine Works is all about minimizing clicks and maximizing the insights. From the landing page, users can easily drill down into the dashboard of a specific machine train with a single click, making it easy to access more in-depth information for high-priority assets. This seamless transition from the overview to the individual asset’s dashboard makes it simple to navigate through equipment details without wasting time.
Visual Recognition and Asset Status at a Glance
The design of the dashboard isn’t just functional; it’s visually intuitive. AMS Machine Works includes graphics specifically designed to make machine identification quick and easy. For example, if a critical alarm is detected on a gearbox, users can instantly recognize the issue visually. By clicking into the gearbox provides an immediate breakdown of measurement locations, measurement points, and measured parameters that triggered the alarm—making it easier than ever to locate and address problems.
Real-Time Data and Recent Values
For maintenance professionals, having access to up-to-the-minute data is crucial. The new AMS Machine Works dashboard presents the most recent measurement values for each piece of equipment, giving users a live look at asset performance. This real-time data is especially helpful for tracking the health of critical components, allowing for faster response to emerging issues.
Contextual Launch for Vibration Analysis
One of the most exciting features of the new dashboard is the contextual launch capability for the vibration analysis tool. Users can launch this advanced tool directly from the dashboard, whether they’re looking at a trend, measurement point, or specific machine parameter. The contextual launch functionality means that users can go directly from identifying a potential issue to analyzing vibration data in a browser-based tool, without having to navigate through additional menus or applications. This streamlined process enables users to dive deep into root cause analysis with minimal friction, accelerating decision-making and facilitating quicker resolutions.
Multi-Level Access to Critical Details
AMS Machine Works understands the need for flexibility. The new dashboard allows users to interact with information at various levels, from a high-level machine train overview down to specific measurement points and individual parameters. This multi-level access gives users the freedom to choose how detailed they want their insights to be, providing everything from a quick summary to an in-depth analysis in just a few clicks.